Code/Patch for u-boot that boot from QSPI?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code/Patch for u-boot that boot from QSPI?

ソリューションへジャンプ
2,709件の閲覧回数
juangutierrez
NXP Employee
NXP Employee

timesyssupport would you have some patch that you can share to build and get vybrid u-boot that boots from QSPI?

0 件の賞賛
返信
1 解決策
2,269件の閲覧回数
juangutierrez
NXP Employee
NXP Employee

I have created a couple of patches on top of Timesys u-boot for make it bootable from QSPI (for TWR board)

For building it. After apply the patches make a clean build.

make clean

make vybrid_config

make u-boot

make u-boot.imx

The u-boot.imx output image file is ready to be flashed into QSPI.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,270件の閲覧回数
juangutierrez
NXP Employee
NXP Employee

I have created a couple of patches on top of Timesys u-boot for make it bootable from QSPI (for TWR board)

For building it. After apply the patches make a clean build.

make clean

make vybrid_config

make u-boot

make u-boot.imx

The u-boot.imx output image file is ready to be flashed into QSPI.

0 件の賞賛
返信
2,269件の閲覧回数
timesyssupport
Senior Contributor II

Hello Juan,

Unfortunately, the current u-boot 2011.12 does not support QSPI-NOR boot. TFTP/NFS, SD, and NAND boot are the current supported boot options.

Thanks,

Timesys Support

2,269件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you help on this case?

0 件の賞賛
返信