Can I boot using QuadSPI from QSPI1?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I boot using QuadSPI from QSPI1?

ソリューションへジャンプ
1,714件の閲覧回数
richarddonkin
Contributor III

I know it is possible to boot using QSPI0, with one or two flash chips. But is it possible to boot using QSPI1?

タグ(2)
0 件の賞賛
返信
1 解決策
1,473件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Yes, you can. Note however that you cannot use parallel mode with QuadSPI1 as there are not the pins for it on the chip. If you want to use parallel (8-bit) mode, you must use QuadSPI0.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,473件の閲覧回数
naoumgitnik
Senior Contributor V

Dear Richard,

The details of your application are a bit unclear, but, please, take a look at another discussion in which you might find an answer - https://community.freescale.com/thread/309836.

Regards, Naoum Gitnik.

1,474件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Yes, you can. Note however that you cannot use parallel mode with QuadSPI1 as there are not the pins for it on the chip. If you want to use parallel (8-bit) mode, you must use QuadSPI0.

0 件の賞賛
返信
1,473件の閲覧回数
richarddonkin
Contributor III

Thank you for the clear response!

0 件の賞賛
返信