Can I boot using QuadSPI from QSPI1?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I boot using QuadSPI from QSPI1?

Jump to solution
2,515 Views
richarddonkin
Contributor III

I know it is possible to boot using QSPI0, with one or two flash chips. But is it possible to boot using QSPI1?

Tags (2)
0 Kudos
Reply
1 Solution
2,274 Views
anthony_huereca
NXP Employee
NXP Employee

Yes, you can. Note however that you cannot use parallel mode with QuadSPI1 as there are not the pins for it on the chip. If you want to use parallel (8-bit) mode, you must use QuadSPI0.

View solution in original post

0 Kudos
Reply
3 Replies
2,274 Views
naoumgitnik
Senior Contributor V

Dear Richard,

The details of your application are a bit unclear, but, please, take a look at another discussion in which you might find an answer - https://community.freescale.com/thread/309836.

Regards, Naoum Gitnik.

2,275 Views
anthony_huereca
NXP Employee
NXP Employee

Yes, you can. Note however that you cannot use parallel mode with QuadSPI1 as there are not the pins for it on the chip. If you want to use parallel (8-bit) mode, you must use QuadSPI0.

0 Kudos
Reply
2,274 Views
richarddonkin
Contributor III

Thank you for the clear response!

0 Kudos
Reply