After using LPRUN mode to display a clock on an LCD, returning to normal mode crashes.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

After using LPRUN mode to display a clock on an LCD, returning to normal mode crashes.

Jump to solution
1,432 Views
brianpaterson
Contributor III

During normal mode, it displays. All is well. We go to LPRUN mode to save power and only show a clock on the LCD

During LPRUN, the clock displays but on exiting back to normal mode, the DCU gives an under-run error condition. LCD goes black, system crashes.

System clock during LPRUN is set to 24MHz. Almost all peripherals are disabled.

Any thoughts?

Thanks,

Brian

0 Kudos
Reply
1 Solution
1,351 Views
brianpaterson
Contributor III
0 Kudos
Reply
1 Reply
1,352 Views
brianpaterson
Contributor III

Solved it.

0 Kudos
Reply