Access DCU registers from User space

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Access DCU registers from User space

ソリューションへジャンプ
2,811件の閲覧回数
riz1231
Contributor I

Hello,


We are not able to access DCU memory mapped registers from user mode (non-privileged) on Vybrid.  Is there any specific settings we have to perform to make it happen?


Note: we are trying to access DCU registers starting from 0x40058000 address (Vybrid Reference Manual, Rev. 7, 06/2014 Page 3034)

Thanks,

Rizwan Rasheed

ラベル(1)
0 件の賞賛
返信
1 解決策
2,468件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
2,469件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
2,469件の閲覧回数
rendy
NXP Employee
NXP Employee

Hi,

please download Vybrid Security Reference manual. There read mainly chapter #5 and chapter #7. There you will get more information about the CSU unit, which should allow you to set access rights to various NIC masters/slaves. If you have further questions, write them here and mention me (character '@' + my name).

Regards

Rene

2,469件の閲覧回数
kenmacfarlane
Contributor III

@ReneKolarik, does MQX support user & supervisor modes? I'm told that There is no user-mode/supervisor-mode split in Vybrid

0 件の賞賛
返信
2,469件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Were you able to acces the registers in user-mode.

Would you be nice enough to share your solution?

Best Regards,

Alejandro

0 件の賞賛
返信
2,469件の閲覧回数
VilemZ
NXP Employee
NXP Employee

Hello,

How can you tried access to registers? And do you read section "55.7 Register protection" on VYBRIDRM? It can be helpful.

Best Regards

Vilem

2,469件の閲覧回数
kenmacfarlane
Contributor III

55.7 is about "Timing, Error and Interrupt Management" in Vybrid Reference Manual, Rev. 5, 07/2013. Has a section on Register protection been introduced? Perhaps this will explain why code that previously worked on a bare metal DCU demo, does not change the DCU registers (albeit on an MQX-based application).

0 件の賞賛
返信
2,468件の閲覧回数
VilemZ
NXP Employee
NXP Employee

Hi Kenneth,

In Vybrid Reference Manual rev. 7, 06/2014 is 55.7 about Register protection.

Vilem

0 件の賞賛
返信