About QSPI clock setting .

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About QSPI clock setting .

ソリューションへジャンプ
2,027件の閲覧回数
takashitakahash
Contributor III

Hi community.

I refered VYBRIDRSERIESEC_Rev_7.pdf of p58"9.5.1 QuadSPI timing".

The QSPI_MCR [DDR_EN] a set (to 1b)in the state, if sent  the command Programing of "SDR", then

I am recognized as to the operation of p59 of "QuadSPI Output / Write timing (SDR mode)" .

whether I should refer to either the operating conditions of this case,

Of p59 "QuadSPI Output / Write timing (SDR mode)" or of p61 "QuadSPI Output / Write timing (DDR mode)"

Whitch referred to either of?

In operatively "SDR mode", SCK  is within the range in the current setting of 69.88MHz in MAX80MHz,
However, when referring to "DDR mode", since the MAX has a 45MHz, it will over the upper limit.

Please teach me SCK setting is no problem at 69.88MHz.

And would you please replay of previous question of ( I want to calculate  of  ”Read freaquency calculations", "Max read frequency", "Hold timing").

ラベル(1)
0 件の賞賛
返信
1 解決策
1,791件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi Takashi,

In case you are configuring the QSPI module in SDR you should refer to table 49 which states that the max SCK frequency is 80MHz. Therefore the 69.88MHz won't be an issue as long as you are working in SDR mode.

Best Regards,

Alejandro

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,792件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi Takashi,

In case you are configuring the QSPI module in SDR you should refer to table 49 which states that the max SCK frequency is 80MHz. Therefore the 69.88MHz won't be an issue as long as you are working in SDR mode.

Best Regards,

Alejandro

0 件の賞賛
返信