I want to calculate of ”Read freaquency calculations", "Max read frequency", "Hold timing"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I want to calculate of ”Read freaquency calculations", "Max read frequency", "Hold timing"

Jump to solution
1,908 Views
takashitakahash
Contributor III

Hi community.

I'm trying to calculate the VYBRIDRSERIESEC_Rev_7.PDF p60 "Read freaquency calculations","Max read frequency","Hold timing", but I don't know following values

Would you please teach me  measured in each of the same kind of value .

・Flash access time

・flash_access(min)

・flash_data_valid(min)

Labels (1)
0 Kudos
Reply
1 Solution
1,735 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

As far I as I see the timings you need are dependant on the QSPI memory you are using.

Therefore you will need to check the timings in your memory.

For example

Frequency calculator guideline (Max read frequency): SCK > (Flash access time)max + (Tis)max

Tis allowed for our QSPI module is a min of 4.5ns.  But Flash access time may be found in the manufacturer datasheet.

/Alejandro

View solution in original post

0 Kudos
Reply
1 Reply
1,735 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

As far I as I see the timings you need are dependant on the QSPI memory you are using.

Therefore you will need to check the timings in your memory.

For example

Frequency calculator guideline (Max read frequency): SCK > (Flash access time)max + (Tis)max

Tis allowed for our QSPI module is a min of 4.5ns.  But Flash access time may be found in the manufacturer datasheet.

/Alejandro

0 Kudos
Reply