About AC spec for SDHC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About AC spec for SDHC

3,230 Views
keisukewatanabe
Contributor III

Dear support,

I have a question about AC spec of SDHC in datasheet p,76.

1.

Does the value of SD2 and SD3 not have the frequency dependence?

When I use it in 25Mhz, I suppose the minimum to be 7ns, I think whether matching does not match the SD side.

Please teach it when other value include frequency dependence.

2.

When SD6 is maximum 8.3ns and SD2 is minimum 7ns, I think that can not output the signal by the next rise.

Is the rise of SD6 reliable by a fall?

Best regards,

Keisuke Watanabe

Labels (1)
0 Kudos
Reply
6 Replies

2,976 Views
naoumgitnik
Senior Contributor V

Dear Keisuke,

I guess we are talking about an interface used with an SDHC card.

May you be more design-specific, please?

Is your Vybrid-based design experiencing any issues while communicating with a card? If so, then what card type, in which circumstances, etc., please?

Sincerely, Naoum Gitnik.

0 Kudos
Reply

2,976 Views
keisukewatanabe
Contributor III

Dear Naoum,

About Table 61. SDHC switching specifications, I am considered as follows.

When SD1 is 50MHz, SD2 and SD3 is 7ns.

When SD1 is 25Mhz, SD2 and SD3 is 17ns.

SD2=SD3 : According to datasheet.

SD4=SD5: According to datasheet.

i.e. SD1=SD2+SD3+SD4+SD5

Is this idea right?

Best regards,

Keisuke

0 Kudos
Reply

2,976 Views
naoumgitnik
Senior Contributor V

Dear Keisuke,

Unfortunately, it is quite difficult to know all the details from the Reference Manual counting a few thousand pages, e.g. timing requirements for standard interfaces usually copied from their specifications.

Based on my experience, much more efficient is focusing on actual problems observed in the customers' designs.

Sincerely, Naoum Gitnik.

0 Kudos
Reply

2,976 Views
keisukewatanabe
Contributor III

Dear Naoum,

I will ask the same question again.

================

About Table 61. SDHC switching specifications, I am considered as follows.

When SD1 is 50MHz, SD2 and SD3 is 7ns.

When SD1 is 25Mhz, SD2 and SD3 is 17ns.

SD2=SD3 : According to datasheet.

SD4=SD5: According to datasheet.

i.e. SD1=SD2+SD3+SD4+SD5

Is this idea right?

================

Does it mean that it is difficult to reply this question?

Best regards,

Keisuke Watanabe

0 Kudos
Reply

2,976 Views
karina_valencia
NXP Apps Support
NXP Apps Support

naoumgitnik can you continue with the follow up on this case?

0 Kudos
Reply

2,976 Views
keisukewatanabe
Contributor III

Dear Naoum,

I think that there is a conflict in the Table 61. SDHC switching specifications of datasheet.

In the following cases, I think the data will be not valid.

SD1=50Mhz

SD2=7ns

SD6=8.3ns(max)

In this case, what is the workaround?

Please tell me, if this idea is wrong.

Best regards,

Keisuke Watanabe

0 Kudos
Reply