128-bit unique chip identifier

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

128-bit unique chip identifier

ソリューションへジャンプ
1,999件の閲覧回数
falstaff
Senior Contributor I

Hi,

According to the Reference Manual Rev. 7, Chapter 2.2 Feature Set, the device supports a "128-bit unique chip identifier". However, the only unique chip identifier I found so far is the 64-Bit long "Device Unique ID" in the fuses (OCOTP_CFG0 and OCOTP_CFG1). Is there another unique ID or is the feature set wrong about the length of this unique chip identifier?

--

Stefan

0 件の賞賛
返信
1 解決策
1,683件の閲覧回数
jiri-b36968
NXP Employee
NXP Employee

Hi Stefan,

there is "only" 64-bit unigue ID on the Vybrid (OTP Bank 0 word 1 and 2). 128 bit can be achieved by combining this and some unused space in OTP block.

But generally just 64 unigue ID from the factory.

/Jiri

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,684件の閲覧回数
jiri-b36968
NXP Employee
NXP Employee

Hi Stefan,

there is "only" 64-bit unigue ID on the Vybrid (OTP Bank 0 word 1 and 2). 128 bit can be achieved by combining this and some unused space in OTP block.

But generally just 64 unigue ID from the factory.

/Jiri

0 件の賞賛
返信
1,683件の閲覧回数
billpringlemeir
Contributor V

Vybrid Security manual Table 6-2. BOOT eFuse Descriptions mentions some sub-field definitions.  If the sub-fields are correct then you can verify if chips are from a similar run.