Why can't I find an IVT at location 0x400 of the demo SD card supplied with Tower Vybrid module

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Why can't I find an IVT at location 0x400 of the demo SD card supplied with Tower Vybrid module

跳至解决方案
1,455 次查看
alanball
Contributor III

Trying to work out why an SD card built from scratch won't boot

Looking at the demo card (which boots fine) there is no recognisable IVT at 0x400 (this area is all 0)

Anyone know why?

Also posted in Vybrid community

0 项奖励
回复
1 解答
1,355 次查看
alanball
Contributor III

OK - my fault

I was mounting the SD card as a disk in the hex editor - I guess this was causing it (or the USB driver ?) to hide anything not in a partition

Dumping the SD card to a file using dd and looking at that reveals the expected IVT

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,356 次查看
alanball
Contributor III

OK - my fault

I was mounting the SD card as a disk in the hex editor - I guess this was causing it (or the USB driver ?) to hide anything not in a partition

Dumping the SD card to a file using dd and looking at that reveals the expected IVT

0 项奖励
回复