code posted in forum messages question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

code posted in forum messages question

Jump to solution
5,813 Views
russellsher
Contributor III

Hi All

Forgive my ignorance but how does one view the code posted in messages which appears as a single line with a scroll bar?

for example at:  https://community.freescale.com/message/37833#37833

Is it possible to expand this out?

Russell

1 Solution
5,411 Views
Monica
Senior Contributor III

Hello Rusell!

The script has been edited in the very same post, please let me know if it is useful that way.

There might be some human errors. If you'd like to have the code in a text document please ask for it.

Regards!

View solution in original post

0 Kudos
Reply
3 Replies
5,412 Views
Monica
Senior Contributor III

Hello Rusell!

The script has been edited in the very same post, please let me know if it is useful that way.

There might be some human errors. If you'd like to have the code in a text document please ask for it.

Regards!

0 Kudos
Reply
5,415 Views
russellsher
Contributor III

Many thanks will do

5,415 Views
Paul_Kuhn
NXP Employee
NXP Employee

This is an issue with the data migration when we brought post from our old platform to this platform.  The only way to correct it is for the original poster to edit the post or to add a new post with the formatted content.  I will see if we can find someone hear at Freescale who can provide an edited version.

0 Kudos
Reply