code posted in forum messages question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

code posted in forum messages question

跳至解决方案
5,825 次查看
russellsher
Contributor III

Hi All

Forgive my ignorance but how does one view the code posted in messages which appears as a single line with a scroll bar?

for example at:  https://community.freescale.com/message/37833#37833

Is it possible to expand this out?

Russell

1 解答
5,423 次查看
Monica
Senior Contributor III

Hello Rusell!

The script has been edited in the very same post, please let me know if it is useful that way.

There might be some human errors. If you'd like to have the code in a text document please ask for it.

Regards!

在原帖中查看解决方案

0 项奖励
回复
3 回复数
5,424 次查看
Monica
Senior Contributor III

Hello Rusell!

The script has been edited in the very same post, please let me know if it is useful that way.

There might be some human errors. If you'd like to have the code in a text document please ask for it.

Regards!

0 项奖励
回复
5,427 次查看
russellsher
Contributor III

Many thanks will do

5,427 次查看
Paul_Kuhn
NXP Employee
NXP Employee

This is an issue with the data migration when we brought post from our old platform to this platform.  The only way to correct it is for the original poster to edit the post or to add a new post with the formatted content.  I will see if we can find someone hear at Freescale who can provide an edited version.

0 项奖励
回复