code posted in forum messages question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

code posted in forum messages question

ソリューションへジャンプ
5,806件の閲覧回数
russellsher
Contributor III

Hi All

Forgive my ignorance but how does one view the code posted in messages which appears as a single line with a scroll bar?

for example at:  https://community.freescale.com/message/37833#37833

Is it possible to expand this out?

Russell

1 解決策
5,404件の閲覧回数
Monica
Senior Contributor III

Hello Rusell!

The script has been edited in the very same post, please let me know if it is useful that way.

There might be some human errors. If you'd like to have the code in a text document please ask for it.

Regards!

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
5,405件の閲覧回数
Monica
Senior Contributor III

Hello Rusell!

The script has been edited in the very same post, please let me know if it is useful that way.

There might be some human errors. If you'd like to have the code in a text document please ask for it.

Regards!

0 件の賞賛
返信
5,408件の閲覧回数
russellsher
Contributor III

Many thanks will do

5,408件の閲覧回数
Paul_Kuhn
NXP Employee
NXP Employee

This is an issue with the data migration when we brought post from our old platform to this platform.  The only way to correct it is for the original poster to edit the post or to add a new post with the formatted content.  I will see if we can find someone hear at Freescale who can provide an edited version.

0 件の賞賛
返信