Using Email with the Community

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using Email with the Community

1,671 Views
dereksnell
NXP Employee
NXP Employee

The Freescale Community allows you to receive email for new content, as well as create new content directly from email.  When used, you can treat content similar to email threads.  But it has the added benefits of members choosing what they follow, and also creating a repository of information that can be searched by any members.

You can customize your Community Email settings, and you can use this guide for more details Changing Your Email Notifications and Preferences.  If you want to receive an email for each individual post to keep up with all activity, then you will need to change your default settings.  To do so,

  1. Go to your preferences, using the pull-down menu in the upper right corner of the web page:
    Preferences.png
  2. Ensure everything in your Community Inbox is emailed to you by setting the Inbox setting to On:
    Inbox.png
  3. You can then follow any group or member, to keep up with all the Activity.  The Follow button is in the upper-right corner of the web page.  When you receive an email from a discussion, you can respond directly to the email, and your response will be posted to the discussion.
    Follow.png
  4. For more general information about using the Community, like Following, refer to Using Freescale Community.

Another great feature to take advantage of is creating new discussions by email.  With this feature, you can send an email, and it will automatically create a new discussion.  Follow these steps to set it up:

  1. Go to the group or project you wish to follow, for example Kinetis Microcontrollers
  2. Find the Actions box, usually on the right side of the page.  Select "Create by Email"
    Actions.png
  3. A dialog box will open.  You can get a contact for your email client with the email address to use when you create new content.  Select the type of content you are interested, usually Discussion.  Then you can receive a vcard file.
    Content.png
  4. Once you have the vcard, save the contact in your email client.  Now you can email that contact, and create content automatically in any group or project.
Tags (1)
0 Kudos
Reply
0 Replies