Inbox AND Firefox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
14,468件の閲覧回数
oaf
Contributor IV

Hi,

Today the entry to the inbox is NOT available when using Firefox (This entry is written via IE)

1 解決策
13,765件の閲覧回数
oaf
Contributor IV

Hi,

Yes, I've tried your suggestion. The suggestion was good, and I can inform you that the culprit is Ghostery V-5.4.5.1 :smileydevil:

I've added the freescale community as an exception to Ghostery and now Firefox is working

(This replay is done from it).

Thx

元の投稿で解決策を見る

20 返答(返信)
13,765件の閲覧回数
admin
Specialist II

Hi, can you please provide a screenshot of the error message you get in Firefox?

0 件の賞賛
返信
13,765件の閲覧回数
oaf
Contributor IV

Inbox.jpgHi,

Enclosed is a screendump when I press the down-arrow beside the blue circle.

I'm using Firefox 37.0.2

0 件の賞賛
返信
13,765件の閲覧回数
oaf
Contributor IV

The start page differs too:

IE.jpg

Firefox.jpg

0 件の賞賛
返信
13,765件の閲覧回数
admin
Specialist II

So, you are not seeing any options after clicking on the arrow?

arrow.png

0 件の賞賛
返信
13,766件の閲覧回数
oaf
Contributor IV

Hi,

1. That's correct, pressing the down-arrow doesn't do anything (except making the background a little bit darker, but this is because of the shift of focus)

2. 2nd problem is that the selection for i.MX, Kinetis... is NOT visible when browsing with Firefox...

0 件の賞賛
返信
13,765件の閲覧回数
admin
Specialist II

Thanks for the detail, let me contact the support team and get back to you.

Plus, can you please let me know your PC's operating system? Or are you accessing from a Tablet or Mobile device?

0 件の賞賛
返信
13,765件の閲覧回数
admin
Specialist II

Also, can you try deleting your cache from Firefox browser and try again?

Besides that, let me know if you can access the menu using other browsers such as Chrome, Safari or IE.

0 件の賞賛
返信
13,765件の閲覧回数
oaf
Contributor IV

Hi,

I'm running Win7-64. I don't have any additional browser except FireFox.

FireFox doesn't work (tried just now)

IE works.... :smileysad:

0 件の賞賛
返信
13,765件の閲覧回数
admin
Specialist II

Hi, it seems like you have Java script disabled.

1.- Go to Firefox browser and type about:config

2.- Press I'll be careful, I promise

Screen Shot 2015-05-19 at 13.50.57.png

3.- Search for javascript.enabled and ensure that is set to true

Screen Shot 2015-05-19 at 13.50.34.png

0 件の賞賛
返信
13,765件の閲覧回数
oaf
Contributor IV

Ok, javascript.enabled was enabled, and yes I've checked my Firefox doesn't work today (either)

about_config.jpg

0 件の賞賛
返信
13,765件の閲覧回数
admin
Specialist II

Do you see any errors in the browser's javascript console when you click the button?

This is how you access the console:

1.- Right Click in the community page

2.- Click on "Inspect Element (Q)"

inspect.png

3.- Make sure you selected the "Console" tab and the "JS" output.

4.- Please share the console errors you get

console.png

0 件の賞賛
返信
13,765件の閲覧回数
oaf
Contributor IV

Hi,

The console is absolute blank, also the coloumn with 'i.MX','Kinetis'... is NOT presentJavaConsole.jpg

0 件の賞賛
返信
13,765件の閲覧回数
admin
Specialist II

Hi, I was wondering if you can join a webex call tomorrow. We’ll be meeting with the verdor.

10am CST – 10:30am CST

OR

11amCST – 11:30am CST

Please confirm.

0 件の賞賛
返信
13,765件の閲覧回数
oaf
Contributor IV

Hi,

Sorry, I was in meetings all day. I have a little problem with scheduling a webex meeting, but I could do kind of dump/experiment if you tell me what to do....

0 件の賞賛
返信
13,765件の閲覧回数
admin
Specialist II

Hi, I was wondering if you had been able to fix the issue and access the community from Firefox?

13,766件の閲覧回数
oaf
Contributor IV

Hi,

Yes, I've tried your suggestion. The suggestion was good, and I can inform you that the culprit is Ghostery V-5.4.5.1 :smileydevil:

I've added the freescale community as an exception to Ghostery and now Firefox is working

(This replay is done from it).

Thx

13,725件の閲覧回数
admin
Specialist II

Awesome! :smileyhappy:

0 件の賞賛
返信
13,765件の閲覧回数
admin
Specialist II

Go to Firefox menu, located at the top right and select Add-ons

ffmenu.png

Click on the Extensions tab and Disable them

ext.png

dis.png

Test access to Community menus again.

0 件の賞賛
返信
13,765件の閲覧回数
admin
Specialist II

Have you recently installed any Addons in Firefox? Can you please try disabling them?

We have just found an Addon called  "Privacy badger" to be causing this issue or any other pop-up blocker...

0 件の賞賛
返信
13,765件の閲覧回数
Ben
Senior Contributor I

Hi Karla,

I am using Firefox too and it works good. However, I am using ver. 34.0. A colleague just lately complained that he faced a lot of troubles in entering sites with Firefox, including local banks sites, but it happened after he upgraded to new Firefox version, so I keep working with ver. 34. Ole is working with ver. 37, maybe your development team know something about the late changes they did in Firefox

0 件の賞賛
返信