do opencv support on mpc5604b board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

do opencv support on mpc5604b board?

Jump to solution
1,833 Views
fahmirazak
Contributor II

im doing a project about line follower using CA-84A/C camera. Do opencv support on mpc5604b board to do the image processing part?

here the datasheet for camera: https://www.google.com/url?sa=t&rct=j&q=&esrc=s&source=web&cd=1&cad=rja&ved=0CCwQFjAA&url=https%3A%2...

Labels (1)
0 Kudos
Reply
1 Solution
1,510 Views
admin
Specialist II

You will find openCV support on the higher end multimedia processors like i.MX.  The MPC5604B is optimized for automotive applications so keep that in mind.  That being said, you can still do vision work with it.  Most commonly for the Freescale Cup,  people interface a generic RCA CMOS type cameras.  Here is a good app note describing that process.

View solution in original post

0 Kudos
Reply
1 Reply
1,511 Views
admin
Specialist II

You will find openCV support on the higher end multimedia processors like i.MX.  The MPC5604B is optimized for automotive applications so keep that in mind.  That being said, you can still do vision work with it.  Most commonly for the Freescale Cup,  people interface a generic RCA CMOS type cameras.  Here is a good app note describing that process.

0 Kudos
Reply