do opencv support on mpc5604b board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

do opencv support on mpc5604b board?

ソリューションへジャンプ
1,823件の閲覧回数
fahmirazak
Contributor II

im doing a project about line follower using CA-84A/C camera. Do opencv support on mpc5604b board to do the image processing part?

here the datasheet for camera: https://www.google.com/url?sa=t&rct=j&q=&esrc=s&source=web&cd=1&cad=rja&ved=0CCwQFjAA&url=https%3A%2...

ラベル(1)
0 件の賞賛
返信
1 解決策
1,500件の閲覧回数
admin
Specialist II

You will find openCV support on the higher end multimedia processors like i.MX.  The MPC5604B is optimized for automotive applications so keep that in mind.  That being said, you can still do vision work with it.  Most commonly for the Freescale Cup,  people interface a generic RCA CMOS type cameras.  Here is a good app note describing that process.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,501件の閲覧回数
admin
Specialist II

You will find openCV support on the higher end multimedia processors like i.MX.  The MPC5604B is optimized for automotive applications so keep that in mind.  That being said, you can still do vision work with it.  Most commonly for the Freescale Cup,  people interface a generic RCA CMOS type cameras.  Here is a good app note describing that process.

0 件の賞賛
返信