Is it possible to design a system which measures SPO2 and provides necessary data to control a stepper motor using only these two Dev Kits MED-SPO2 and TWR-S08MM128

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is it possible to design a system which measures SPO2 and provides necessary data to control a stepper motor using only these two Dev Kits MED-SPO2 and TWR-S08MM128

3,049 次查看
shivakumardindu
Contributor I

Hi,  this is Shivakumar a final year B Tech Student. I have planned to do a project on automatic oxygen regulator using pulse oximeter. I have decided to do this project using your Dev Kits i.e MED-SPO2: Pulse Oximeter Development Kit and TWR-S08MM128: MC9S08MM Medical Development Tower System Module.  So would you please  clarify the following query.  1)Is it possible to design a system which measures SPO2 and provides necessary data to control a stepper motor using only these two Dev Kits MED-SPO2 and TWR-S08MM128

0 项奖励
回复
0 回复数