Freescale Innovation Challenge RULES-Timer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Freescale Innovation Challenge RULES-Timer

跳至解决方案
5,094 次查看
For_Seal
Contributor I

Hello Freescale community,

I have a question regarding a timer last lap notification.

Rules content this section:

"The car will be notified about entering the last lap via a row of red LEDs positioned above the start/stop line. Red LEDs mean that the car is entering its last lap. The total number of laps is the same for all teams engaged into the same race event."

so we can use sensor (camera, RGB sensor) to detect last lap, but it is a easier way: set number of laps by button before ride and ignore "semaphore". How you want prevent this way? Or it isn't a breaking the rule?

Thanks for answer

标签 (2)
0 项奖励
回复
1 解答
4,764 次查看
FlavioStiffan
NXP Employee
NXP Employee

The car is notified about when it enters the lap means that it must not be preset into the car at the time of the start (via pushbutton or any other way for preprogramming. Indeed the car needs to have a light sensor to know when it passes into the last lap.

在原帖中查看解决方案

3 回复数
4,765 次查看
FlavioStiffan
NXP Employee
NXP Employee

The car is notified about when it enters the lap means that it must not be preset into the car at the time of the start (via pushbutton or any other way for preprogramming. Indeed the car needs to have a light sensor to know when it passes into the last lap.

4,764 次查看
For_Seal
Contributor I

Thanks for answer.
When it is breaking the rules...How you want identify purpose of pushing button at the start? I am asking,because we can use buttons for another setting like speed-set or set car to the run mode.

0 项奖励
回复
4,764 次查看
FlavioStiffan
NXP Employee
NXP Employee

Well.... it is the reason it is a pilot program and that we ask for fair-play and honesty in our contests. The only other way would be NOT to say how many laps and make it different for each competitor. I am not sure that it would be a fair race.... but it could be interesting. A good thought for the next year's contest.

0 项奖励
回复