大学项目知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

University Programs Knowledge Base

讨论

排序依据:
Using a "warp drive controller" as a fun example, this video will introduce the audience to basic hardware interfacing concepts, device register documentation and how one interacts with hardware. View Video Link : 1456
查看全文
Find the complete material at: https://community.freescale.com/docs/DOC-95205
查看全文
In this training video we will decompose an NTSC video signal to gaining understanding of how to capture video data from a "analog" camera.
查看全文
Harvard Extension School CSCI E-251, Fall 2012: Principles of Operating Systems Final Project Presentations Presentation by David Lieberman
查看全文
Harvard Extension School CSCI E-251, Fall 2012: Principles of Operating Systems Final Project Presentations Presentation by Kate Fischl
查看全文
Find the complete material at: https://community.freescale.com/docs/DOC-95205
查看全文
This video will examine how can design speed sensing into their vehicle platform.   An example of magnet and sensor placement is shown.
查看全文
Entrenamiento sobre el UART basado en la Familia Kinetis L. Encuentra el material completo en https://community.freescale.com/docs/DOC-95205
查看全文
After formal competition finished in East China, we gave a challenge and asked teams to try a hill with >30 angle, some cars successes
查看全文
The Freescale Cup Brazil 2012 Semifinal and Final National Competition was held on October 25th, 2012 in the Designing with Freescale Market Solutions Seminar Sao Paulo. Universities from all over the country participated in the challenge by creating a high-speed, autonomous, race of RC scale cars. Part of Freescale's University Programs to promote engineering in the classroom... Are you Ready to Participate?
查看全文
Using the logic described in part 2 of the linescan camera tutorial, the actual implementation of the interface will be showed. The example code for the FRDM-TFC shield will be used as a reference implementation of a completely interrupt driven camera interface.
查看全文
Harvard Extension School CSCI E-251, Fall 2012: Principles of Operating Systems Final Project Presentations Presentation by Victor Petrov
查看全文
Line scan camera data processing - Part II
查看全文
Freescale Cup China - Two Wheel Self Balancing Challenge 2012 In China they have another tier of competition in which the cars must complete the track autonomously while balancing on the rear wheels. For this challenge they use a charged wire in the track for which to sense and navigate the vehicle by. Really cool!
查看全文
Compilation of views taken during The Freescale Cup 2015 Worldwide Finals held at the Fraunhofer IIS during the event opening. Credit: Fraunhofer IIS
查看全文
Footage taken using the Fraunhofer IIS Eagle Cam attached to the Car from the Politecnico of Torino on the final track layout. Credit: Fraunhofer IIS
查看全文
Watch the video highlights of the Freescale Cup Worldwide Finals 2015 for the training sessions. Credit: Fraunhofer IIS
查看全文
Footage from the technical inspection taken during The Freescale Cup 2015 Worldwide Finals. Credit: Fraunhofer IIS         
查看全文
Second part in the series showing tips and tricks to getting the most of your line scan camera.
查看全文
Portuguese, Recording of the training provided for The Freescale Cup Brazil 2013 for the Freedom Dev Platform by Denis Shimizu
查看全文