ユニバーシティ・プログラムのナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

University Programs Knowledge Base

ディスカッション

ソート順:
The TWR-K40X256 Kit is a Freescale evaluation board powered by the Kinetis K40 microcontroller. The Kinetis microcontroller family is a set of 32 bit ARM Cortex M4 chips which feature flexible storage, lower power usage, high performance and optional Floating Point Unit with many useful peripherals. For more information on the Kinetis family see Freescale's Kinetis website. The Tower System is a prototyping platform with interchangeable and reusable modules along with open source design files. Freescale K40 MCU Tower Module: TWR K40X256 Hardware Setup There are several main hardware configuration steps. After installing the battery, once the USB cable has been connected between the evaluation board and PC, it may be necessary to update the chip firmware which requires moving a jumper pin on the evaluation board. TWR K40X246 Hardware Setup Instructions Board Specific Tutorials K40 Blink LED K40 Drive DC Motor K40 Drive Servo Motor K40 Line Scan Camera Board Tips The TWR-K40X256 features a socket that can accept a variety of different Tower Plug-in modules featuring sensors, RF transceivers, and more. The General Purpose TWRPI socket provides access to I2C, SPI, IRQs, GPIOs, timers, analog conversion signals, TWRPI ID signals, reset, and voltage supplies. The pinout for the TWRPI Socket is defined in Table 3 of the TWR-K40X256 User's Manual, but the user manual does not describe how to order a connector. A Samtec connector, part number: SFC-110-T2-L-D-A is the proper female mating connector for the TWR-K40X256 TWRPI socket. SIDE A/SIDE B White DOTS for counting Pins Solder Wire to GND, and to MCU VDD Pin for testing purposes Important Documents TWR-K40X256 User's Manual TWR-K40X256 Schematics External Links TWR-K40X256-KIT Webpage Kinetis Discussion Forum Tower Geeks Community Website Tower Geeks Freescale Cup Group
記事全体を表示
En este video puedes consultar paso a paso la descarga e instalación del CodeWarrior 10.4 para microcontroladores. Accede a la liga www.freescale.com/cwmcu10
記事全体を表示
A look at interrupts in a microcontroller from a generic point of view. This will be used to put the other videos relating to interrupts of the ARM core in context.
記事全体を表示
Entrenamiento acerca del MCG de la herramienta de desarrollo Freedom, para los microcontroladores Kinetis L series. Para acceder al material completo visita: https://community.freescale.com/docs/DOC-95205
記事全体を表示
In this training video we will decompose an NTSC video signal to gaining understanding of how to capture video data from a "analog" camera.
記事全体を表示
Video footage highlights taken during The Freescale Cup Worldwide Finals 2015 Award Ceremony Credit: Fraunhofer IIS
記事全体を表示
Illustrates some basic concepts with respect to microcontroller design tools. A generic design flow will be introduced to orient the audience to the most common steps in the software development process.
記事全体を表示
25 student teams from 21 universities coming from 11 countries will meet on 29-30 April for the Freescale Cup EMEA Challenge. Check out the event information at https://www.facebook.com/events/1425416907713292/
記事全体を表示
Congratulations to the winning teams!! First Place Second Place Third Place Mach Pi- Universidade de Sao Paulo Poli - Gryphon- Universidade de Sao Paulo Zohan- Universidade do Estado de Santa Catarina Final Time: 15.52 Final Time: 18.27 Final Time: 20.1 David Nissimoff Diego Negrao Coordinator: Vitor Nascimento William Ricardo Kishimoto Diniz Jéssica Barbosa Heluany Wesley Wein Chen Coordinator: Fuad Kassab Junior Jean Ribeiro Fernandes Marcus Vieira Soares Rodolfo Lauro Weinert Coordinator: Ana Watanabe *Download zip file for more pictures.
記事全体を表示
Freescale Cup China - Two Wheel Self Balancing Challenge 2012 In China they have another tier of competition in which the cars must complete the track autonomously while balancing on the rear wheels. For this challenge they use a charged wire in the track for which to sense and navigate the vehicle by. Really cool!
記事全体を表示
The Freescale Cup East China 2013 challenge video 2 After formal competition finished in East China, we gave a challenge and asked teams to try a hill with >30 angle, some cars successes
記事全体を表示
Have you even wondered where to get started when you wish to get support for your project? Here is a short presentation giving you the links to Project Sponsorship, Freescale Social Networks and other useful resources.
記事全体を表示
Data acquisition system for Kinetis K Family Author : Mauro Padin (Student) Supervisors : Professor Daniel A. Jacoby, Juan Pablo Vega (Teacher Assistant)   Summary:   This project is based on the FRDM-K64F board, a HC-05 Bluetooth module, and a smartphone. In this application, an analog signal is sampled and transmitted wirelessly to a smartphone, using an external Bluetooth module, where it is displayed. The complete CodeWarrior C code and MIT App Inventor code can be found in the .zip file. System Structure SysTick Module: Periodically triggers ADC conversions and UART transmissions. ADC Module: Samples the analog signal and manages the ADC input buffer. UART Module: Manages the UART output buffer and transmits the digitized data. Bluetooth Module: When connected, wirelessly transmits the data coming from the UART module. Smartphone App: Handles Bluetooth connection, receives the digitized data and manages the display.   Software Structure   A project template is provided to the students in order to establish a simple, and easy, program organization for the duration of the course. A portion of the template was built with the help of the Processor Expert so that, later on, the students would be able to understand its structure and limitations, and transition to this new tool. A wrapper was built around this auto-generated code and the resulting function, void __LDM_init (void), is to be used at the very beginning of the project given. This function mainly configures internal processor registers related to clock configuration.   The project is composed of separate files for each hardware and software module:   The template is composed of four files: LDM.c/h, main.c, and misc.h. The application is found in: App.c/h RTI, ADC, UART, LED Drivers are defined in: RTI.c/h, adc.c/h, uart.c/h, and LED.c/h.   The basic Driver structure consists of a void DRV_init(void) initialization, a set of void DRV_x_ISR(void) interrupt handlers, a set of void DRV_x_PISR(void) periodic interrupt handlers, and a set of void DRV_x services function. Only the initialization function is mandatory, the others being optional and dependent on the driver purpose. Service functions are interfaces between the application and the Driver and do not necessarily access any subjacent hardware. Indeed, this Driver structure can be nested and thus not handle any hardware at all. When a Driver function does access hardware, it is recommended to further use a Hardware Abstraction Layer to enhance productivity and improve portability.   Extracts of the system   As an example of the Driver Structure, the LED Driver is described below:   init void LED_init  (void)   ISR N/A   PISR void LED_PISR  (void)    Services void LED_write  (color_t color, bool value) void LED_set  (color_t color) void LED_clear  (color_t color) void LED_toggle (color_t color)   The entire application is interrupt driven, so that only initialization are necessary and the run loop is empty:   void App_init(void) {   LED_init();  // LED driver init function   uart_init();  // UART driver init function   adc_init();  // ADC driver init function   RTI_init();  // RTI driver init function }   void App_run(void) { }       Hardware interrupts are not serviced in their specific handler but referred to external handlers for readability and organization. The SysTick interrupt handler is composed of a ISR and a Service:   ISR_t SysTick_Handler(void) {   LED_isr code   ADC_conv code } The code for the smartphone side is depicted below:     Finally, a screenshot of the result:       Original Attachment has been moved to: -ADC-bluetooth-TP6.zip
記事全体を表示
Lecture 1: Introduction and Motor Basics  This training module presented by Professor L. Umanand of CEDT, Indian Institute of Science, Bangalore provides an overview of the Freescale Cup – 2011. It introduces to the challenge describing the various components of the intelligent car tracker. Lecture 2: Pulse Width Modulation  This lecture provides an overview of Pulse Width Modulation Lecture 3: Control Design  This lecture describes controller design and PID control Lecture 4: Speed and Position  This Lecture discusses integrating your PID with sensor data Lecture 5: MPC5607B Overview  This training module provides an overview of the 32-bit Qorivva MPC5607B Processor. The course is targeted towards beginners in order to enable them to quick start the development of software on the MPC5607B.
記事全体を表示
Congratulations to the Winning Teams!! First Place Second Place Third Place Team Chrysler Team Ford Team Panasonic 23.91 seconds 26.80 seconds 27.34 seconds Team Members: Tom Pruett Sandhya Etikala Manjiri Joshi Team Members: Saumil Patwari Jim Weinfurther Kevin Hille Team Members: Vince Li Jeffery Kuo Adeel Yusuf The complete times are listed below.
記事全体を表示
32-bit Kinetis MCUs represent the most scalable portfolio of ARM® Cortex™-M4 MCUs in the industry. Enabled by innovative 90nm Thin Film Storage (TFS) flash technology with unique FlexMemory (configurable embedded EEPROM), Kinetis features the latest low-power innovations and high performance, high precision mixed-signal capability. For the Freescale Cup Challenge, we have provided several tutorials, example code and projects based on the twr-k40x256-kit. This board is part of the Freescale tower-system, a modular, reusable development platform that allows engineers to quickly prototype new designs. The K40 chip is a 144 pin package with 512KB of Flash, 245Kb of Program Flash, 4KB of EEProm, and 64KB of SRAM. Important Documents: Reference Manual Besides the Reference manual and the Datasheet, the most useful document for learning to program the K40 chip is the Kinetis Peripheral Module Quick Reference Data sheet Errata External Links Freescale's Kinetis K40 Product Page
記事全体を表示
1. Download CodeWarrior 2.8 Evaluation Version (Classic, Windows-hosted) To Program your microcontroller you will need to set up the CodeWarrior Integrated Development Environment. CodeWarrior is available on the Freescale.com Website. Method 1: Direct Link direct download link (Caution - link may not be up to date) Method 2: Navigate to the Download Link From Freescale.com click on: "Design Resources" tab at the top of the page, then navigate to "Software and Tools", and then to "Codewarrior Devleopment Tools" Click on the "Download CodeWarrior now link" Click on the Download Evaluation Versions link" Within this page, use your browser "find" feature (Typically CTRL-F) to search for the text string "V2.8" Click the "download" button next to "Evaluation: CodeWarrior for MPC55xx/MPC56xx Microcontrollers V2.8 (Classic)". and save it to your computer. 2. Install CodeWarrior To install CodeWarrior Development Studio for Microcontrollers v2.8, double-click the installation package and a wizard will guide you through the installation process. Installation Notes: Are you using Windows Vista or Windows 7? Evaluation Edition User: If you are installing the Evaluation Edition, the Evaluation license is automatically installed with your product and you do not need to register it. This license allows you to develop projects as Professional Edition within the 30-day evaluation period. After 30 days, the license works as Special Edition license (free permanent, but feature limited) which supports unlimited assembly code, up to 32KB of C code for HCS08/RS08 derivatives, up to 64KB of C code for V1 ColdFire derivatives and up to 128KB of C code for V2-V4 ColdFire and Kinetis derivatives and up to 512KB of C code for MPC56xx derivatives. Once you have finished downloading and installing CodeWarrior, users can return to Downloading and Installing P&E as part of the Blink a LED on Qorivva Tutorial
記事全体を表示
Entrenamiento sobre ADC del Kinetis L Series. Encuentra el material completo en https://community.freescale.com/docs/DOC-95205
記事全体を表示