TFC - EMEA - wall comments

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TFC - EMEA - wall comments

Jump to solution
62,657 Views
FlavioStiffan
NXP Employee
NXP Employee
6-TFC_Logo_sizes.jpg

32 schools and over 300 students have registered for the 2012/2013 Freescale Cup competition across 9 countries. 

This year the race will feature a choice of 2 MCU platforms:

  • Qorivva's MPC5604B 32bit Automotive controller
  • Kinetis ARM Cortex-M4 32bit Industrial microcontroller

Students are working to create the most intelligent race car to win the EMEA Finals that will be held end of March 2013 at the ESIEE Paris. Follow their progress and see their videos on this site.

0 Kudos
1 Solution
61,602 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this discussion as solved, due to a migration of a new community platform.
If you have additional questions, please create a new post and reference to this closed thread.

NXP Community!

View solution in original post

0 Kudos
120 Replies
61,603 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this discussion as solved, due to a migration of a new community platform.
If you have additional questions, please create a new post and reference to this closed thread.

NXP Community!
0 Kudos
14,853 Views
admin
Specialist II

I will look into.

0 Kudos
14,848 Views
Grandpierre
Contributor II

Hello,

On the wiki page "K40: Line Scan Camera Tutorial"  (http://freescalecupwiki.freescale.com/en:k40-line-scan-camera )  a link is missing to the zip archive for the camera example project for the tower K40.

Similarly, on the K40: Blinking LED (http://freescalecupwiki.freescale.com/en:k40-blink-led) the link to the example code "LED_BLINK_96MHZ" is broken.

Best regards,

Thierry

0 Kudos
14,853 Views
FlavioStiffan
NXP Employee
NXP Employee

Hi Marek,

No, the boards are standard for all the competitors. There is a choice of the MPC5604B TRK board, the K40 tower, K40 Kwikstik and a new board with integrated motor control featuring K40 that will be available in July. All the data is already loaded in the Wiki on StreetSmarts

0 Kudos
14,853 Views
admin
Specialist II

Thank you. So we will be able to make custom control boards with that processor for this year?

0 Kudos
14,854 Views
FlavioStiffan
NXP Employee
NXP Employee

Hi Matthieu, 

yes, the track's specs are the same as last year but we are adding some new MCU platforms to the competition. See the new discussion started for the next season.

0 Kudos
14,854 Views
MatthieuB_
Fresh Out Contributor

Hello,

we are thinking about the next cup, and we would like to know whether the line width will be the same next year. Could you tell us if any changes are forecasted ?

Thank you

0 Kudos
14,854 Views
FlavioStiffan
NXP Employee
NXP Employee
Marek, the tunnel has a 30cm clearance
0 Kudos
14,854 Views
admin
Specialist II

Hello. Would like to know what high was the tunnel / max high of car. Cant find it anywhere. Thank you.

0 Kudos
14,854 Views
FlavioStiffan
NXP Employee
NXP Employee

highlights video is posted

on StreetSmarts

0 Kudos
14,844 Views
FlavioStiffan
NXP Employee
NXP Employee

All, find attached the final results of the race per team

Finals.pdf

0 Kudos
14,844 Views
RichardBalogh_n
Contributor II

Flavio, please can You provide us with the detailed results (all teams, times achieved) also with a qualification results? If possible, I would like to see the team videos once more (at least the winning one). Thanks for great event!

0 Kudos
14,844 Views
FlavioStiffan
NXP Employee
NXP Employee
Richard, if the documentation has changed, a change list is sufficient. Thanks
0 Kudos
14,844 Views
RichardBalogh_n
Contributor II

Question about the documentation update: should the team provide completely new (updated) documentation, or just changelist?

0 Kudos
14,844 Views
FlavioStiffan
NXP Employee
NXP Employee

Each car goes through 1 round of qualification (2 times 1 lap) but as we have 34 teams, it will take us some time to get through this on Tuesday afternoon and Wednesday morning to give time to each time to do it. Technically, if you go all the way to the final round, your car will go 4 times around the track: 2 times 1 lap in Qualification and 2 times 1 lap during the final round

0 Kudos
14,844 Views
PrzemysawKochas
Contributor I

Does "Start of 1st Qualifications", "Cont'd 1st Qualifications" and "Cont'd 1st Qualifications" on the next day mean that (1) each robot has to participate in every qualification session and go through 2 laps in each one of them or (2) each team has to participate in only one of that sessions?

0 Kudos
14,844 Views
FlavioStiffan
NXP Employee
NXP Employee

@Sorin: no changes.... you will meet the official track in Prague!! Safe travels

0 Kudos
14,844 Views
SorinCracana
Contributor I

4. Width of the racing track shall not be less than 600mm/23.65in.

6. Surface of the racing track is matte white, with a continuous black line (25mm/1in wide) drawn in the middle as the pilot line.

7. The minimum bending radius of the racing track shall not be less than 500mm/19.7in.

9. Any slope in the track will be equal to or less than 15 degrees in a straight section of the racing track, including upgrade and downgrade.
10. There is a straight starting area of 1000mm/39.4in long in the racing track, as shown in figure below. In addition, there is a black starting line 100mm/3.9in long at both sides of the starting point. Start time and end time will be determined when the front part of the racing car passes the starting line. The car must be able to automatically

Is any of these changed?

0 Kudos
14,844 Views
FlavioStiffan
NXP Employee
NXP Employee
@ Cracana: yes they are. Which point are you unsure of?
0 Kudos
14,844 Views
SorinCracana
Contributor I

Do the " Section 11: Parameters of the Racing Track " from the TFC_2011_RULES_EMEA v3 still apply to the contest ?

0 Kudos