Searching for a Motor Drive Version-A Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Searching for a Motor Drive Version-A Board

1,553件の閲覧回数
zylkaadam
Contributor I

Hi,

our team is searching for the Motor Drive Version-A Board. We can't find it neither on the freescale homepage nor on other sides.

Does anybody have this board and doesn't use it? We would be very appreciated to buy it.t

Greetings

Adam

タグ(3)
0 件の賞賛
2 返答(返信)

813件の閲覧回数
FlavioStiffan
NXP Employee
NXP Employee

Adam, the current TFC-Shield is now available online for ordering. It can be connected to the Qorivva MPC560xB board. All the schematics for the connectivity are available (see Thread above).

0 件の賞賛

813件の閲覧回数
FlavioStiffan
NXP Employee
NXP Employee

Hi Adam,

The boards are no longer manufactured but all the schematics are available to create your own. Link on the Freescale Community's Freescale Knowledge Database at Freescale Cup Motor Driver Board

The H-Bridge MC33931 is available for free sampling on our Freescale.com site at MC33931 Product Summary Page

0 件の賞賛