Searching for a Motor Drive Version-A Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Searching for a Motor Drive Version-A Board

1,258 Views
zylkaadam
Contributor I

Hi,

our team is searching for the Motor Drive Version-A Board. We can't find it neither on the freescale homepage nor on other sides.

Does anybody have this board and doesn't use it? We would be very appreciated to buy it.t

Greetings

Adam

Tags (3)
0 Kudos
2 Replies

518 Views
FlavioStiffan
NXP Employee
NXP Employee

Adam, the current TFC-Shield is now available online for ordering. It can be connected to the Qorivva MPC560xB board. All the schematics for the connectivity are available (see Thread above).

0 Kudos

518 Views
FlavioStiffan
NXP Employee
NXP Employee

Hi Adam,

The boards are no longer manufactured but all the schematics are available to create your own. Link on the Freescale Community's Freescale Knowledge Database at Freescale Cup Motor Driver Board

The H-Bridge MC33931 is available for free sampling on our Freescale.com site at MC33931 Product Summary Page

0 Kudos