what is the T2080 DDR validation CWTAP id

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

what is the T2080 DDR validation CWTAP id

4,985件の閲覧回数
muaxi8
Contributor V

T2080rdb, I need DDR Validation, but I can't connect the target, because I don't know how to fill in the

CWTAP ID.

muaxi8_0-1655297168572.png

 

0 件の賞賛
返信
11 返答(返信)

4,980件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

For CodeWarrior TAP USB connection, no need to specify CWTAP id.

For CodeWarrior Ethernet connection, please click target connections->Edit, specify Probe address as CodeWarrior TAP IP address.

 

0 件の賞賛
返信

4,967件の閲覧回数
muaxi8
Contributor V

i  use the CodeWarrior TAP USB connection,I tried to read the parameters from SPD, but the following

error occurred:

Target is not ready: Target does not respond and/or could not be reset

 

muaxi8_0-1655696245341.png

 

0 件の賞賛
返信

4,914件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please execute the following command in CCS console

% source IDCode.tcl

% delete all

% config cc cwtap

% ccs::config_chain t2080

% ccs::reset_to_debug

0 件の賞賛
返信

4,773件の閲覧回数
muaxi8
Contributor V

i use a usb codewarrior tap. I followed the steps you said, but the connection failed.The following is the CCS log。

 

(bin) 55 % source IDCode.tcl

Scanning for available TAPs connected via USB.....


++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
+
+ Available Remote Connections
+
+ 1 - CodeWarriorTAP - 00:04:9f:06:15:f8
+ 2 - CodeWarriorTAP - <Specify IP Address>
+ 3 - EthernetTAP - <Specify IP Address>
+ 4 - GigabitTAP - <Specify IP Address>
+
+ x - Exit Script without Changes
+
++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++

Specify connection:
1

Configuring TAP Interface....

Configured Connection: cwtap : 00:04:9f:06:15:f8


TDO -----
|
* Device 0 IDCODE: 018E701D Device: FSL T2080 rev 1.x
|
TDI -----


###################################################
#
# configTAP - Redefine TAP interface
#
# scanboard - Scans the target system
# and returns the JTAG IDCode
#
# ir - Loopback test
#
###################################################

(bin) 55 % delete all
(bin) 56 % config cc cwtap
(bin) 57 % ccs::config_chain t2080
(bin) 58 % ccs::reset_to_debug

0 件の賞賛
返信

4,761件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

There is no problem with the basic connection between CodeWarrior and the target board.

When you click "Read SPD", CCS(CodeWarrior Connection Server) will be popped up at the right bottom of the Window task bar, please open CCS console and type "log v", then click "Read SPD" again, the low level CCS log will be printed out in the CCS console. Would you please capture this CCS log to me to do more investigation.

0 件の賞賛
返信

4,754件の閲覧回数
muaxi8
Contributor V

there is  no  output

muaxi8_0-1660205251321.png

 

0 件の賞賛
返信

4,725件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please close CodeWarrior IDE and all CCS consoles.

Please open CodeWarrior IDE in a new workspace, then create a QCVS DDR project.

Please click "Read SPD", CCS(CodeWarrior Connection Server) will be popped up at the right bottom of the Window task bar, please open CCS console and type "log v", then click "Read SPD" again, the low level CCS log will be printed out in the CCS console automatically.

Would you please capture this CCS log to me to do more investigation?

0 件の賞賛
返信

4,723件の閲覧回数
muaxi8
Contributor V

 I closed CodeWarrior IDE and all CCS consoles;

I open CodeWarrior IDE in a new workspace, then create a QCVS DDR project.

I clicked "Read SPD", CCS popped up at the right bottom of the Window task bar,  i opened CCS console and type "log v", then click "Read SPD" again, but there is nothing in ccs. my god

muaxi8_0-1660532265883.png

 

0 件の賞賛
返信

4,720件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to my following CCS log, even not plug in CodeWarrior TAP to the PC.

(bin) 1 % log v
CCS Windows Release Build 439p0
verbose logging
CCSAPI connection #1 accepted from NXL65555.wbi.nxp.com at Mon Aug 15 11:55:25 2022
check_min_version(serverh=0,*version)
api version: 00000004 00000006
available_connections(serverh=0,*count,*cc)
connections: {0,73,0x00000000}
cc_version(serverh=0,cc_index=0,index=0,*version)
ERROR(64): CC config string is invalid
CCSAPI connection #1 from NXL65555.wbi.nxp.com closed at Mon Aug 15 11:55:25 2022
(bin) 2 %

 

Did you install QorIQ Configuration and Validation Suite 4.5.0.0001-20160210?

You could get the version information from Help->Install New Software->already installed.

Or please try to uninstall QCVS tool and reinstall it again, please don't plug in CodeWarrior TAP when installing the software.

0 件の賞賛
返信

4,717件の閲覧回数
muaxi8
Contributor V

codewarrior version is 10.5

i  have  installed QorIQ Configuration and Validation Suite 4.5.0.0001-20160210 .

muaxi8_1-1660541139578.png

 

0 件の賞賛
返信

4,711件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

It seems that your QCVS IDE cannot communicate with CCS.

Please try to reinstall CodeWarrior and QCVS. Please try to install them in another PC if necessary.

Please download CodeWarrior for PA 10.5.1 from the following link.

链接: https://pan.baidu.com/s/18bzcYKQsZaPrJOz8lkR9uw?pwd=dy4a 提取码: dy4a 

Please download QCVS for PA 4.5 from the following link.

链接: https://pan.baidu.com/s/11sMsNdnr8zPp7IHhn_FLig?pwd=c3bi 提取码: c3bi 

Please don't plugin CodeWarrior TAP during installation.

0 件の賞賛
返信