t4240rdb boot error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

t4240rdb boot error

2,584件の閲覧回数
varunkjayan
Contributor II

i have loaded a new image fsl-image -core changing conf to add gcc,make etc

and the file size is big

when i load the file the file shows that the file

error fs ext2 :u image cannot be defined 10755 fsl-image minimal

and also showing

error at stack 0x701 iam not able to boot my system

please help

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,444件の閲覧回数
Pavel
NXP Employee
NXP Employee

Do you use the ext2.gz.u- boot file of the fsl-mage-core file system?


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,444件の閲覧回数
varunkjayan
Contributor II

yes

0 件の賞賛
返信

2,444件の閲覧回数
Pavel
NXP Employee
NXP Employee

Try to use fsl-image-full for your changing.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信