t4240rdb boot error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

t4240rdb boot error

2,577 次查看
varunkjayan
Contributor II

i have loaded a new image fsl-image -core changing conf to add gcc,make etc

and the file size is big

when i load the file the file shows that the file

error fs ext2 :u image cannot be defined 10755 fsl-image minimal

and also showing

error at stack 0x701 iam not able to boot my system

please help

标签 (1)
0 项奖励
回复
3 回复数

2,437 次查看
Pavel
NXP Employee
NXP Employee

Do you use the ext2.gz.u- boot file of the fsl-mage-core file system?


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,437 次查看
varunkjayan
Contributor II

yes

0 项奖励
回复

2,437 次查看
Pavel
NXP Employee
NXP Employee

Try to use fsl-image-full for your changing.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复