t4240 ddr validation target connections fail

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

t4240 ddr validation target connections fail

跳至解决方案
3,081 次查看
muaxi8
Contributor V

t4240 custom board. 

Now my board is stuck in the DDR initialization section, so I  created a DDR project using

CodeWarrior, but CodeWarrior cannot connect to the DDR. 

CodeWarrior Debug can connect, DDR verification is not,why? 

Can you check my CW configuration for me

muaxi8_0-1659606684969.png

I want to know if my connection configuration is correct ?

muaxi8_0-1659606296071.png

 

 

0 项奖励
回复
1 解答
3,015 次查看
yipingwang
NXP TechSupport
NXP TechSupport

It seems that you didn't open the correct CCS console.

Please close CodeWarrior IDE and all CCS consoles.

Then open CodeWarrior IDE again, click Target Connection, the CCS console will be popped up automatically, please use this CCS console, type "log v" and connect to the target board again, the low level CCS log will be printed out.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,055 次查看
yipingwang
NXP TechSupport
NXP TechSupport

When you click "Start Validation" the CCS(CodeWarrior Connection Sever) will be popped up at the right bottom of the Window task bar, please open CCS console, type "log v" then click "Start Validation" again, the low level CCS log will be printed in CCS console, please capture this CCS log to me to do more investigation.

0 项奖励
回复
3,053 次查看
muaxi8
Contributor V

 

My current problem is that the "Start Validation" is grayed out and I can't click on it

muaxi8_0-1660041846027.png

 

0 项奖励
回复
3,042 次查看
yipingwang
NXP TechSupport
NXP TechSupport

You use T4240 processor, why did you configure the "System" as T2080?

If your problem remains, please capture the CCS log to me to do more investigation.

 

0 项奖励
回复
3,040 次查看
muaxi8
Contributor V

I have two boards, a T2080RDB and a T4240 custom board.

t4240 custom boadr is discrete ddr.

No output is generated after the target connection.

muaxi8_0-1660207029869.png

 

muaxi8_1-1660207054995.png

 

this is my  codewarrior.  I don't know because something is wrong with the configuration ?

muaxi8_1-1660209871900.png

 

 

0 项奖励
回复
3,016 次查看
yipingwang
NXP TechSupport
NXP TechSupport

It seems that you didn't open the correct CCS console.

Please close CodeWarrior IDE and all CCS consoles.

Then open CodeWarrior IDE again, click Target Connection, the CCS console will be popped up automatically, please use this CCS console, type "log v" and connect to the target board again, the low level CCS log will be printed out.

0 项奖励
回复