qemu run with kvm enable and does not run without it

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

qemu run with kvm enable and does not run without it

1,236件の閲覧回数
pirooz_najafi1
Contributor I

qemu runs guest os ok with kvm enable but does not run with kvm disable. Do you guys see anything wring with these options.

 

Ron’s ok, I see the os initialization and I can run nbench program and measure performance of 99.5% effecient

qemu-system-ppc64 -enable-kvm -m 4096 -nographic -M ppce500 -kernel /boot/uImage -initrd /nsdl/fsl-image-virt-t4240rdb-64b-20200121045736.rootfs.ext2.gz -append "root=/dev/ram rw console=ttyS0,115200" -serial tcp:192.168.0.210:5505,server,telnet

 

 

don’t aee any terminal print on guest os. Only difference is

qemu-system-ppc64  -m 4096 -nographic -M ppce500 -kernel /boot/uImage -initrd /nsdl/fsl-image-virt-t4240rdb-64b-20200121045736.rootfs.ext2.gz -append "root=/dev/ram rw console=ttyS0,115200" -serial tcp:192.168.0.210:5505,server,telnet

 

When I trace the code, it looks like I am getting trap location 4.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,146件の閲覧回数
bpe
NXP Employee
NXP Employee

You need KVM to run QUEMU on  a PowerPC machine running SDK generated
binaries. Fully userspace emulation is in theory possible but not verified/
supported.

Regards,

Platon

0 件の賞賛
返信