how to create rcw project with codewarrior 10.5 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to create rcw project with codewarrior 10.5 ?

984 次查看
muaxi8
Contributor V

I am using t4080 custom board and I want to know how to create RCW project with CodeWarrior 10.5

0 项奖励
回复
1 回复

976 次查看
yipingwang
NXP TechSupport
NXP TechSupport

T4080 is a single core cluster variant of T4240(3 clusters) and T4160(2 clusters). T4080 is smaller version of T4160. T4080 has four dual threaded Power Architecture e6500 cores with the same two memory complexes(CoreNet platform cache and DDR3 memory controller) with the same high-performance datapath acceleration, networking, and peripheral bus interfaces.

 

So the customer could use T4160 CodeWarrior project to connect to T4080 board. Please refer to the attached initialization file, only reducing the number of cores is needed.

0 项奖励
回复