how to create rcw project with codewarrior 10.5 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to create rcw project with codewarrior 10.5 ?

1,017 Views
muaxi8
Contributor V

I am using t4080 custom board and I want to know how to create RCW project with CodeWarrior 10.5

0 Kudos
Reply
1 Reply

1,009 Views
yipingwang
NXP TechSupport
NXP TechSupport

T4080 is a single core cluster variant of T4240(3 clusters) and T4160(2 clusters). T4080 is smaller version of T4160. T4080 has four dual threaded Power Architecture e6500 cores with the same two memory complexes(CoreNet platform cache and DDR3 memory controller) with the same high-performance datapath acceleration, networking, and peripheral bus interfaces.

 

So the customer could use T4160 CodeWarrior project to connect to T4080 board. Please refer to the attached initialization file, only reducing the number of cores is needed.

0 Kudos
Reply