/dev/ttyUSB0 not created

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

/dev/ttyUSB0 not created

4,628 Views
sujas
Contributor I

Hi,

I have to connect 4G LTE module L506 to  T1024 based board as a USB device. Kernel is configured with following configuration:

CONFIG_USB_SERIAL=y
CONFIG_USB_SERIAL_CONSOLE=y
CONFIG_USB_SERIAL_GENERIC=y

/dev/ttyUSB0 entry is not present. Decvice ID and vender ID is also provided in  drivers/usb/serial/option.c file. Please help to resolve this issue.

SDK version 1.9

Kernel Version : 3.12 RT 51+

Thanks & Regards,

Labels (1)
0 Kudos
Reply
3 Replies

4,281 Views
vinothkumars
Senior Contributor IV

Are you sure about this /dev/ttyUSB0? Maybe you got some other device entry also.

Regards,

VinothS

Regards,
Vinothkumar Sekar
0 Kudos
Reply

4,280 Views
Pavel
NXP Employee
NXP Employee

Is "USB Serial Converter support" enabled in kernel menu?

See attached Clipboard02.jpg file.

Find configuration for your device in kernel menu for your device. See attached Clipboard04.jpg file.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,280 Views
sujas
Contributor I

Yes, It is enabled.

Thanks for the reply,

0 Kudos
Reply