dTSEC and PTP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,464件の閲覧回数
bogdantanasa
Contributor II

Hi,

I am curious about the accuracy that one can achieve when using PTP to do time synchronization in the context of a T4240 CPU running Linux Yocto. According to the Reference Manual, the CPU is equipped with dTSEC capability (and not eTSEC). Would the accuracy be better or worse if T4240 would have had a eTSEC interface?

Thanks,

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
3,917件の閲覧回数
bpe
NXP Employee
NXP Employee

The timestamping unit and IEEE 1588 adjustable timer on eTSEC and

dTSEC are very much similar. Different is only how timestamps are

conveyed to the software, through DPAA or not. This does not

significantly affect the accuracy. Practically achievable numbers

depend on both the network and software implementation. Contact your

distributor or FAE for performance information.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,917件の閲覧回数
bogdantanasa
Contributor II

Thanks!

I am curious if QorIQ SDK 1.6 enables the hardware timestamping capabilities of the dTSEC in a T4240. Inspecting the manual (QorIQ-SDK-1.6-IC-RevB.pdf) in Section 8.14.1.6 only the dpaa_1588.c, dpaa_1588.h and dpaa_eth.c files are listed. In contrast, when comparing with QorIQ-SDK-1.9-IC-RevA in Section 7.9.1 one more file is listed dpaa_ptp.c.

Does the PTPd stack in SDK 1.9 allows for better accuracy compared to SDK 1.6 (which seems to miss one)?

0 件の賞賛
返信
3,918件の閲覧回数
bpe
NXP Employee
NXP Employee

The timestamping unit and IEEE 1588 adjustable timer on eTSEC and

dTSEC are very much similar. Different is only how timestamps are

conveyed to the software, through DPAA or not. This does not

significantly affect the accuracy. Practically achievable numbers

depend on both the network and software implementation. Contact your

distributor or FAE for performance information.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,917件の閲覧回数
bogdantanasa
Contributor II

What technical document one can read about dTSEC, timestamping unit and their interaction with Linux Yocto?

Thanks,

0 件の賞賛
返信
3,917件の閲覧回数
bpe
NXP Employee
NXP Employee

For hardware-level details, refer to T4240DPAARM, Chapter 7, for SDK support details visit the following links:

Submit Form

Submit Form

Note that T4240 DPAA-controlled multi-rate Ethernet interfaces are not dTSECs, they are next generation peripherals

called mEMAC.

0 件の賞賛
返信