Need help in DPAA driver development on T1024

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need help in DPAA driver development on T1024

1,729件の閲覧回数
veerendranathj
Contributor III

Hi,

Can anyone share some reference code for bare board DPAA driver development on T1024RDB...

As I my requirement is develop bare-board drivers development.. I can't use SDK...

Thanks and Regards,

Veerendranath

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,392件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello veerendranath jakkam,

Please download NetComm Software from NetComm Software Resources|NXP , it is a bareboard software drivers package, uses CodeWarrior as the development tool, you could download GA 4.7.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信