Virtual core in T-series processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Virtual core in T-series processor

跳至解决方案
1,139 次查看
prasantahalder
Contributor II

Hi,

In the datasheet of quad core t1042 processor, I found that it's core virtual core. Does that mean t has two physical core with hyper threading? If not, what is the difference between virtual core and physical core?

Thanks in advance.

Regards,

Prasanta

标签 (1)
标记 (1)
1 解答
1,019 次查看
alexander_yakov
NXP Employee
NXP Employee

The t1042 processor core (e5500 core) does not support multi-threading, this feature is available starting from e6500 core.

So, in case of t1042 "virtual core" is equal to "physical core" - t1042 device has 4 physical cores. This is said in T1040 Reference Manual, Table 1-1 and, also, shown at Figure 1-2:

pastedImage_1.png

Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,020 次查看
alexander_yakov
NXP Employee
NXP Employee

The t1042 processor core (e5500 core) does not support multi-threading, this feature is available starting from e6500 core.

So, in case of t1042 "virtual core" is equal to "physical core" - t1042 device has 4 physical cores. This is said in T1040 Reference Manual, Table 1-1 and, also, shown at Figure 1-2:

pastedImage_1.png

Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------