UART/USB mux configuration in Yacto dts file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

UART/USB mux configuration in Yacto dts file

跳至解决方案
1,432 次查看
vinothkumars
Senior Contributor IV

Dear NXP Friends,

         I am currently working on UART/USB/etc in T4160RDB-64B machine. I want to configure uart in dts file. But, in yacto dts files are different with normal one for mux pin configuration. 

         Please provide any document or steps to understand yacto dts file configuration for mux pin.

Regards,

VinothS

Regards,
Vinothkumar Sekar
标签 (1)
0 项奖励
回复
1 解答
1,298 次查看
Pavel
NXP Employee
NXP Employee

Try to configure these pins assigning in the u-boot for the T4160RDB.


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,299 次查看
Pavel
NXP Employee
NXP Employee

Try to configure these pins assigning in the u-boot for the T4160RDB.


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,298 次查看
vinothkumars
Senior Contributor IV

Hi Pavel,

Thank you for your reply. As per your suggestion the mux pin configuration for T4160RDB machine in U-Boot side,

Is it right?

Regards,
Vinothkumar Sekar
0 项奖励
回复