UART/USB mux configuration in Yacto dts file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART/USB mux configuration in Yacto dts file

Jump to solution
1,435 Views
vinothkumars
Senior Contributor IV

Dear NXP Friends,

         I am currently working on UART/USB/etc in T4160RDB-64B machine. I want to configure uart in dts file. But, in yacto dts files are different with normal one for mux pin configuration. 

         Please provide any document or steps to understand yacto dts file configuration for mux pin.

Regards,

VinothS

Regards,
Vinothkumar Sekar
Labels (1)
0 Kudos
Reply
1 Solution
1,301 Views
Pavel
NXP Employee
NXP Employee

Try to configure these pins assigning in the u-boot for the T4160RDB.


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,302 Views
Pavel
NXP Employee
NXP Employee

Try to configure these pins assigning in the u-boot for the T4160RDB.


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,301 Views
vinothkumars
Senior Contributor IV

Hi Pavel,

Thank you for your reply. As per your suggestion the mux pin configuration for T4160RDB machine in U-Boot side,

Is it right?

Regards,
Vinothkumar Sekar
0 Kudos
Reply