T4241 IFC Timing parameters for Normal GPCM with ext acknowledge based access does the programmable timing values in IFC_FTIMx_CSn_GPCM apply?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T4241 IFC Timing parameters for Normal GPCM with ext acknowledge based access does the programmable timing values in IFC_FTIMx_CSn_GPCM apply?

1,593 Views
williamweishaup
Contributor II

When Using Normal GPCM mode in the Acknowledgment mode (WGETA and RGETA = 1) are the control signal timing values still based on the programmed values in the IFC_FTIMn_CSn_GPCM except for Twp and Trad?  The Reference manual is not clear in this area because the timing diagrams shown for a Acknowledgment Mode write (Figure 12-44) and  read (Figure 12-49) do not shown the programable timing values. The figures for the internal counter based program operation mode Figure 12-40 (write) and Figure 12-47 (Read) show the programmed values.

Labels (1)
0 Kudos
Reply
1 Reply

1,403 Views
ufedor
NXP Employee
NXP Employee

> When Using Normal GPCM mode in the Acknowledgment mode (WGETA and RGETA = 1)

> are the control signal timing values still based on the programmed values in the

> IFC_FTIMn_CSn_GPCM except for Twp and Trad?

Yes.

0 Kudos
Reply