T4160 SD card interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T4160 SD card interface

1,962件の閲覧回数
logifrancis
Contributor III

I have a T4160 based board, in which i am testing the SD card interface. In the uboot shell, when i type mmc info command it is giving the response as "Card did not respond to voltage select!" . SD card I am using is Sandisk micro SD HC class1 16GB card. In my board i have used a voltage translator to convert 1.8V to 3.3V (card side) . When I probed the SD clock, it is at 400Khz. 

What could be the issue? Is there a provision at uboot to disable voltage selection?

0 件の賞賛
返信
1 返信

1,844件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Logi Francis,

 

"Card did not respond to voltage select" is caused by failure of the ACMD41, which means that the voltage selection settings by the host does not match with eMMC device.

Please check RCW configuration.

SDHC_BASE (371): 0;

SPI_BASE (382-383): 01 to use 8-bit eMMC support;


Please refer to the attached schematics on T2080QDS.

Please try increase your timeout value SYSCTL[DTOCV] to be E.

Thanks,

Yiping

0 件の賞賛
返信