T4160 SD card interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T4160 SD card interface

1,961 次查看
logifrancis
Contributor III

I have a T4160 based board, in which i am testing the SD card interface. In the uboot shell, when i type mmc info command it is giving the response as "Card did not respond to voltage select!" . SD card I am using is Sandisk micro SD HC class1 16GB card. In my board i have used a voltage translator to convert 1.8V to 3.3V (card side) . When I probed the SD clock, it is at 400Khz. 

What could be the issue? Is there a provision at uboot to disable voltage selection?

0 项奖励
回复
1 回复

1,843 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Logi Francis,

 

"Card did not respond to voltage select" is caused by failure of the ACMD41, which means that the voltage selection settings by the host does not match with eMMC device.

Please check RCW configuration.

SDHC_BASE (371): 0;

SPI_BASE (382-383): 01 to use 8-bit eMMC support;


Please refer to the attached schematics on T2080QDS.

Please try increase your timeout value SYSCTL[DTOCV] to be E.

Thanks,

Yiping

0 项奖励
回复