T2081: Enabling MAC10 for 1G speed in u-boot level

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T2081: Enabling MAC10 for 1G speed in u-boot level

810 次查看
noufalp90
Contributor III

Hi All,

In my design, we have 1G ethernet connected to Processor side.(T2081). I want to enable MAC10 interface instead of MAC4 for RGMII connection. Can anyone help me to bring up MAC10 interface with RGMII in u-boot level

 

 

Thanks,

Noufal

 

T2080 

0 项奖励
回复
3 回复数

772 次查看
LFGP
NXP TechSupport
NXP TechSupport
dear @noufalp90,

you have to set some fields into the RCW, please review the chapter "3.4.11 Ethernet controller 2 and GPIO3 signal multiplexing" to get the whole details.
0 项奖励
回复

771 次查看
LFGP
NXP TechSupport
NXP TechSupport
into the T2080RM please
0 项奖励
回复

792 次查看
noufalp90
Contributor III

Hi,

Anyone can guide me how can I enable the Mac10 in u-boot level for T208x ??

In my project, we are able to see linkup for only 100Mbps. But as per errata "A-009057: MAC4 does not support 10/100Mbps operation when connected to the RGMII interface", it is mentioned that MAC4 does not support 10/100mbps, only MAC3 and MAC10 is supported. So I would like to configure either MAC3 or MAC10 as default ethernet for us. 

0 项奖励
回复