T2080rdb-pc non-ecc so-dimm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080rdb-pc non-ecc so-dimm

Jump to solution
7,228 Views
tapyang
Contributor III

Dear Engineers of NXP:

I am using the T2080RDB-PC board, and found a problem about the DDR.

I changed the DDR3 memory card(original=D3XP56082XL10AA)

pastedImage_1.png

with my laptop memory card(RMT3150ED58E8W1600).

pastedImage_2.png

Then, It doesn't work any more.

I have considered the 1.35V(DDR3L) and 1.5V(DDR3) , tried others laptop memory card(about five kinds of memory card), and get the same results.

I saw the register of DDR below, and it is fine!

pastedImage_3.png

I used the DDRv tool to validate them, and would't get the right value.

pastedImage_4.png

However, the original DDR3L works fine in 1066M/1333M/1600M/1866M, and could find the right value in DDRv tool.

pastedImage_5.png

I also tried the 4GB DDR3L laptop memory card, and It couldn't work too.

Theonly difference is that D3XP56082XL10AA support ECC and RMT3150ED58E8W1600 cann't support ECC...

Does the T2080RDB-PC only support the ECC memory card?Why my memory card can't work?

Looking forward to your reply, and Best wishes to you!

                                                                                                                               Yours sincerely

Labels (1)
0 Kudos
Reply
1 Solution
6,943 Views
ufedor
NXP Employee
NXP Employee

In the provided SO-DIMM datasheet it is written:

● 204-pin Dual-in-line DDR3 memory module.
● JEDEC Standard with 1.5 V (±0.075 V) power supply

View solution in original post

0 Kudos
Reply
5 Replies
6,943 Views
ufedor
NXP Employee
NXP Employee

Please provide U-Boot log and datasheet for the SO-DIMM in question.

0 Kudos
Reply
6,939 Views
tapyang
Contributor III

OK, Thanks for your reply!

And the U-BOOT log and the SO-DIMM DDR3 datasheet see the attachments.

Expect your reply, thx.

 

0 Kudos
Reply
6,939 Views
ufedor
NXP Employee
NXP Employee

Please provide the SO-DIMM datasheet.

0 Kudos
Reply
6,939 Views
tapyang
Contributor III

OK! I found the  SO-DIMM datasheet finally, see the attachment please.

0 Kudos
Reply
6,944 Views
ufedor
NXP Employee
NXP Employee

In the provided SO-DIMM datasheet it is written:

● 204-pin Dual-in-line DDR3 memory module.
● JEDEC Standard with 1.5 V (±0.075 V) power supply

0 Kudos
Reply