T2080 cache partition

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 cache partition

2,366 Views
daeilkang
Contributor I

Dear All

I am going to devlop the system by using T2080 and VxWorks 653 3.0 version.

I will use the fsl_t2080_qds evaluation board from freescale.

Question 1>

The L2 cahe of T2080 is shared among foru physical cores.

Is there any way to partition the L2 Cache to each core??

Please let me know how to do that.

Question 2>

There are two memac ports (memac 2 and memac 3) in t2080 QDS board.

I want to test different network configuration with this board.

First, I want to configure that  only one core can hanle tow memac ports.

What shall I do this?

Second, I also wanto to configure that first core hansles memac2, and second core handles memac3, respectively.

What shall I do this?

Third, If I want to add another memac port, like memac4.

What shall I do this?

If you have any query, please do not hesitate to ask me.

Thanks in advance.

Kang.

Labels (1)
0 Kudos
Reply
1 Reply

2,031 Views
Pavel
NXP Employee
NXP Employee

1) Look at the Section 2.12.4 of the e6500 Core Reference Manual:

http://cache.nxp.com/files/32bit/doc/ref_manual/E6500RM.pdf?fsrch=1&sr=2&pageNum=1

2) It looks like that these questions are specific to VxWorks. If NXP SDK is used, see kernel configuration using kernel menu and .dts file.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply