T2080 DDR3 problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T2080 DDR3 problem

3,609 次查看
xiaopengma
Contributor I

I use tcl to initial DDR3 Controller,

I open Memory Broswer,the value is ???????.

157888_157888.jpgQQ图片20160804112020.jpg

What is wrong?

Here is my tcl file.

Original Attachment has been moved to: T2080QDS_init_core.tcl.zip

标签 (1)
0 项奖励
回复
3 回复数

3,392 次查看
addiyi
NXP Employee
NXP Employee

In your init file, did you config DDR to starts from 0x0?

Adrian

0 项奖励
回复

3,392 次查看
xiaopengma
Contributor I

Thanks,Adrian.

This should be a RCW issue.

0 项奖励
回复

3,390 次查看
Pavel
NXP Employee
NXP Employee

I have tested simple CodeWarrior project on the T2080rdb board. See attached screenshot. Test your board using attached project.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复