T2080 DDR3 problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 DDR3 problem

3,512 Views
xiaopengma
Contributor I

I use tcl to initial DDR3 Controller,

I open Memory Broswer,the value is ???????.

157888_157888.jpgQQ图片20160804112020.jpg

What is wrong?

Here is my tcl file.

Original Attachment has been moved to: T2080QDS_init_core.tcl.zip

Labels (1)
0 Kudos
Reply
3 Replies

3,295 Views
addiyi
NXP Employee
NXP Employee

In your init file, did you config DDR to starts from 0x0?

Adrian

0 Kudos
Reply

3,295 Views
xiaopengma
Contributor I

Thanks,Adrian.

This should be a RCW issue.

0 Kudos
Reply

3,293 Views
Pavel
NXP Employee
NXP Employee

I have tested simple CodeWarrior project on the T2080rdb board. See attached screenshot. Test your board using attached project.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply