T2080 CGA_PLL1_RAT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 CGA_PLL1_RAT

2,112件の閲覧回数
scottgerhold
Contributor IV

We are running SYSCLK at 100MHz. We are using PLL1 to drive the FMAN. We use Processor Expert to create the RCW. In the past I have been able to set CGA_PLL1_RAT to 7:1. But now it appears I cannot set it lower than 8:1. Did PE change to limit the value? The reference manual states 5:1 is allowed, but states look elsewhere (datasheet is assumed) to determine limitations.

In the datasheet, Table 121 discusses PLL frequencies. I may have missed the limitation there in the past as I assume it was for the Core frequency, does that require the CGA_PLL1 and CGA_PLL2 to meet a minimum of 1000MHz? 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

2,070件の閲覧回数
ufedor
NXP Employee
NXP Employee

> does that require the CGA_PLL1 and CGA_PLL2 to meet a minimum of 1000MHz? 

Yes.

The Data Sheet requirements must be fulfilled - else normal processor operation is not guaranteed.

0 件の賞賛
返信