T2080 CGA_PLL1_RAT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T2080 CGA_PLL1_RAT

2,143 次查看
scottgerhold
Contributor IV

We are running SYSCLK at 100MHz. We are using PLL1 to drive the FMAN. We use Processor Expert to create the RCW. In the past I have been able to set CGA_PLL1_RAT to 7:1. But now it appears I cannot set it lower than 8:1. Did PE change to limit the value? The reference manual states 5:1 is allowed, but states look elsewhere (datasheet is assumed) to determine limitations.

In the datasheet, Table 121 discusses PLL frequencies. I may have missed the limitation there in the past as I assume it was for the Core frequency, does that require the CGA_PLL1 and CGA_PLL2 to meet a minimum of 1000MHz? 

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

2,101 次查看
ufedor
NXP Employee
NXP Employee

> does that require the CGA_PLL1 and CGA_PLL2 to meet a minimum of 1000MHz? 

Yes.

The Data Sheet requirements must be fulfilled - else normal processor operation is not guaranteed.

0 项奖励
回复