T1042RDB bring-up error (error writing memory [CCS last error: Scan timeout])

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1042RDB bring-up error (error writing memory [CCS last error: Scan timeout])

1,917 Views
Ray_33
Contributor II

Please refer to the diagnostic information as attached. Any advice? Thanks.

0 Kudos
Reply
5 Replies

1,869 Views
Ray_33
Contributor II

CodeWarrior Tap is connected over USB as indicated by the starting guide.

I'm using Windows 10, 64 bit OS.

Please feel free to let me know if you need more information. 

1,854 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello Ray_33

Unfortunately, the only connection available is via ethernet for Windows 10, 64 bit OS.

Have a wonderful day,

Best Regards,

Hector Villarruel

0 Kudos
Reply

1,819 Views
Ray_33
Contributor II

Hi Hector,

Thanks for the reply. I did try to configure TAP as ethernet access, but it seems I still got same issue. The connecting status shows good, but once it passed to T1042RDB_init_core.tcl, the debug process will halt with below information: "No source available for "0x00000000FFFFFFFC (0x00000000FFFFFFFC)()". Please see below screenshot.

Any further suggestion? 

Thanks.

Ray_33_0-1678831701757.png

 

 

0 Kudos
Reply

1,782 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello Ray_33
Hope this post finds you well,

Please close CW and delete .metadata folder from your workspace. Then create a new bareboard project using the new project wizard and select T1042. Then download the default application in your board.

What could be the cause of this problem ?
- software installed,
- project,
- interface,
- board.

To check the different point I recommend to use a sample project.
You can create a sample with the project Wizard
File + New + CodeWarrior Bareboard Project Wizard
Here you can create an example with all your hardware configuration: interface + board.
For this test I recommend to use an eval board.
This will valid the Tool installation and Interface.
If this project example is running the problem could be on the project or your own board.

Now you can replace the eval board with your board.
If this example project is running on your board, the problem is linked to your project.

Best Regards,

Hector Villarruel

0 Kudos
Reply

1,878 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello Ray_33

Hope this post finds you well,

Could you please be so kind to answer the following questions?

Could you please provide more details about your connection?

Are connecting the CodeWarrior Tap over USB or Ethernet?

Are you using Windows or linux ?

Which version of linux or Windows are you currently using to perform the test?

I will be waiting for your kind update,

Best Regards,

Hector Villarruel

0 Kudos
Reply