T1042RDB bring-up error (error writing memory [CCS last error: Scan timeout])

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1042RDB bring-up error (error writing memory [CCS last error: Scan timeout])

2,098件の閲覧回数
Ray_33
Contributor II

Please refer to the diagnostic information as attached. Any advice? Thanks.

0 件の賞賛
返信
5 返答(返信)

2,050件の閲覧回数
Ray_33
Contributor II

CodeWarrior Tap is connected over USB as indicated by the starting guide.

I'm using Windows 10, 64 bit OS.

Please feel free to let me know if you need more information. 

2,035件の閲覧回数
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello Ray_33

Unfortunately, the only connection available is via ethernet for Windows 10, 64 bit OS.

Have a wonderful day,

Best Regards,

Hector Villarruel

0 件の賞賛
返信

2,000件の閲覧回数
Ray_33
Contributor II

Hi Hector,

Thanks for the reply. I did try to configure TAP as ethernet access, but it seems I still got same issue. The connecting status shows good, but once it passed to T1042RDB_init_core.tcl, the debug process will halt with below information: "No source available for "0x00000000FFFFFFFC (0x00000000FFFFFFFC)()". Please see below screenshot.

Any further suggestion? 

Thanks.

Ray_33_0-1678831701757.png

 

 

0 件の賞賛
返信

1,963件の閲覧回数
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello Ray_33
Hope this post finds you well,

Please close CW and delete .metadata folder from your workspace. Then create a new bareboard project using the new project wizard and select T1042. Then download the default application in your board.

What could be the cause of this problem ?
- software installed,
- project,
- interface,
- board.

To check the different point I recommend to use a sample project.
You can create a sample with the project Wizard
File + New + CodeWarrior Bareboard Project Wizard
Here you can create an example with all your hardware configuration: interface + board.
For this test I recommend to use an eval board.
This will valid the Tool installation and Interface.
If this project example is running the problem could be on the project or your own board.

Now you can replace the eval board with your board.
If this example project is running on your board, the problem is linked to your project.

Best Regards,

Hector Villarruel

0 件の賞賛
返信

2,059件の閲覧回数
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello Ray_33

Hope this post finds you well,

Could you please be so kind to answer the following questions?

Could you please provide more details about your connection?

Are connecting the CodeWarrior Tap over USB or Ethernet?

Are you using Windows or linux ?

Which version of linux or Windows are you currently using to perform the test?

I will be waiting for your kind update,

Best Regards,

Hector Villarruel

0 件の賞賛
返信