T1042 NOR Boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1042 NOR Boot

3,142件の閲覧回数
mdursun
Contributor II

Hello,

I am trying to boot from NOR FLASH for T1042 processor. Swicthes are set to boot from NOR-FLASH.

I have written the images to the following addresses of NOR flash.

  • 0xE8000000 - PBL.bin ( Generated by QCVS)
  • 0xEFF00000 - FMAN ucode.bin
  • 0xEFF40000 - u-boot-nor-2016.09+fslgit-r0.bin

Initial stage of the boot is being successful, it means that RCW is read from the NOR-flash. However nothing happens after it.

T1042 has a 256kB CPC (that can be configured as SRAM). Since u-boot-nor-2016.09+fslgit-r0.bin is 768kB, I assume that there would be a Secondary Program Loader (SPL).

At first stage an SPL shall be loaded to the CPC from NOR-FLASH. Then SPL,

  • shall initialize the DDR,
  • shall copy U-BOOT.bin from NOR-FLASH to the DDR,
  • shall jump to the U-BOOT code.

However I couldn't find any SPL binary in QORIQ SDK directories. Where can I find this binary file?

 

Best Regards,

Mustafa

0 件の賞賛
返信
5 返答(返信)

3,131件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

u-boot-nor-2016.09+fslgit-r0.bin is 768kB, that is the correct size of whole NOR flash u-boot image.

There is no SPL for NOR FLASH u-boot, u-boot boots directly from NOR flash then initializes DDR and copies u-boot image to DDR and jump executing from DDR.

u-boot provided in QorIQ SDK 2.0 is used for T1042RDB demo board, you need to modify u-boot source code according to your custom board.

DDR controller initialization section provided in SDK 2.0 u-boot for T1042RDB is not suitable for your custom board, you need to modify u-boot source code board/freescale/t104xrdb/ddr.h according to your custom board.

You could refer to this document

https://community.nxp.com/t5/Qonverge-Knowledge-Base/DDR-Controller-Configuration-on-LS2085-LS2080-B...

0 件の賞賛
返信

3,127件の閲覧回数
mdursun
Contributor II

Hi @yipingwang ,

Thanks for the clarification of the SPL issue for NOR-FLASH boot.

Previously, I have changed the DDR.h file according to our custom board DDR and successfully boot u-boot from SDCARD with those settings. I am using same DDR.h file for u-boot-nor-2016.09+fslgit-r0.bin but it stucks.

Following is the list of the files that I have changed to make source codes copliant with our custom-board.

  • T1042D4RDB_defconfig /git/configs
  • t1042d4_sd_rcw.cfg /git/board/freescale/t104xrdb
  • t104x_pbi.cfg /git/board/freescale/t104xrdb
  • law.c /git/board/freescale/t104xrdb
  • ddr.c /git/board/freescale/t104xrdb
  • ddr.h /git/board/freescale/t104xrdb
  • fsl_esdhc_spl.c /git/drivers/mmc

Can there be a setting that effects NOR-boot in above files?

Is there any other required modification on source codes for NOR-boot?

Best Regards,

Mustafa

0 件の賞賛
返信

3,123件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

If you use different IFC NOR flash on your custom board from T1042RDB, you need to modify NOR flash IFC timing configuration section in u-boot.

You need to modify the following section in u-boot source code include/configs/T104xRDB.h.

/* NOR Flash Timing Params */
#define CONFIG_SYS_NOR_CSOR CSOR_NAND_TRHZ_80
#define CONFIG_SYS_NOR_FTIM0 (FTIM0_NOR_TACSE(0x4) | \
FTIM0_NOR_TEADC(0x5) | \
FTIM0_NOR_TEAHC(0x5))
#define CONFIG_SYS_NOR_FTIM1 (FTIM1_NOR_TACO(0x35) | \
FTIM1_NOR_TRAD_NOR(0x1A) |\
FTIM1_NOR_TSEQRAD_NOR(0x13))
#define CONFIG_SYS_NOR_FTIM2 (FTIM2_NOR_TCS(0x4) | \
FTIM2_NOR_TCH(0x4) | \
FTIM2_NOR_TWPH(0x0E) | \
FTIM2_NOR_TWP(0x1c))
#define CONFIG_SYS_NOR_FTIM3 0x0

#define CONFIG_SYS_FLASH_QUIET_TEST
#define CONFIG_FLASH_SHOW_PROGRESS 45 /* count down from 45/5: 9..1 */

#define CONFIG_SYS_MAX_FLASH_BANKS 2 /* number of banks */
#define CONFIG_SYS_MAX_FLASH_SECT 1024 /* sectors per device */
#define CONFIG_SYS_FLASH_ERASE_TOUT 60000 /* Flash Erase Timeout (ms) */
#define CONFIG_SYS_FLASH_WRITE_TOUT 500 /* Flash Write Timeout (ms) */

#define CONFIG_SYS_FLASH_EMPTY_INFO
#define CONFIG_SYS_FLASH_BANKS_LIST {CONFIG_SYS_FLASH_BASE_PHYS}

You could refer to https://community.nxp.com/t5/Layerscape-Knowledge-Base/IFC-Controller-Configuration-on-QorIQ-Custom-...

3,117件の閲覧回数
mdursun
Contributor II

Hi @yipingwang,

Yes we have used different IFC NOR flash on our custom board from T1042RDB.

Before trying to boot from NOR-FLASH, as I previosuly said, I have successfully boot from SDCARD. After this, I have tested and verified that all of the other peripherals on the board, i.e. NAND-flash, PCIe, Ethernet, and NOR-FLASH were working properly.

At that verification step, I had changed the settings(/* NOR Flash Timing Params */) in *include/configs/T104xRDB.h* in order to access NOR-FLASH. (Mostly non-timing related parameters, data width, bank count etc...) Nevertheless, I have executed a full write/read test on IFC-NOR flash, and it was successful. I should also mention that I am writing RCW, FMAN microcode and U-BOOT.bin to the NOR-FLASH by using u-boot commands. (erase, cp.b etc...)

Briefly, I can access IFC NOR-FLASH when I boot from SDCARD, but although same settings are used in u-boot-nor-2016.09+fslgit-r0.bin, it fails to boot from NOR-flash.

I will check the timing parameters to be sure. But does the situation I described above make sense?

Best Regards,

Mustafa

0 件の賞賛
返信

3,106件の閲覧回数
mdursun
Contributor II

Hi @yipingwang ,

The problem is solved in two steps.

  1. Since I was assuming that DDR will be used in NOR-flash, BOOT_LOC was selected as Memory Complex1, in my RCW settings. I changed it to be IFC but this alone did not solve the problem.
  2. Just to try it out, I deleted all the PBI commands added to the end of the RCW. Then it boot from NOR-flash.

Best Regards,

Mustafa

タグ(1)
0 件の賞賛
返信